Back to top

IL.LIMITP and scope

0 votes
+ vote
Vote up!

Hello,

 

Is there a way to have the IL.LIMITP parameter on the scope on AKD Workbench ?

Best regards

 

JLM

0 Comments

1 Answer

0 votes
+ vote
Vote up!

One option is to add the "IL.LIMITP" to the "Watch Window", positioned below the scope. 

Example is attached.

Attachment 

Comments

Thanks a lot.
But I change the IL.LIMITP by EtherCat PDO (0x60E0) in relationship with PL.FB (0x6064), and I want to check this through the scope (the watch window is not fast enough due to the refresh time)
I know that some internal variables could be scoped (like for example 0x2000186e.s16 for the Sin/cos amplitude...) Perhaps there are the same kind of address for IL.LIMITP...

Best regards.

defty - Fri, 01/08/2021 - 06:10
Log in or register to post comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.