Back to top

How is the rated speed of a motor determined

0 votes
+ vote
Vote up!

What defines the rated speed of an AKM motor.

How is the rated speed of a Linear Motor defined.

0 Comments

1 Answer

0 votes
+ vote
Vote up!

The rated speed of a rotary motor is the maximum speed at which the rated torque can be produced continuously before the motor torque starts to roll off sharply.

 

The rated velocity of the linear motor is  the maximum velocity of motor where the rated  force can be produced continuously before the motor's force starts to roll off sharply.

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.