Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

How do I home a motor with an absolute feedback device in the AKD. That is today I hook it up to a load, start moving it to a switch and then call that position zero. Whenever I save that position today, cycle power, a new position comes up. | 30 May 2014 | |

How do I home a motor with an absolute feedback device in the AKD. That is today I hook it up to a load, start moving it to a switch and then call that position zero. Whenever I save that position today, cycle power, a new position comes up.

 

 

Comments & Answers

jcoleman02 said ...

jcoleman02 | Wed, 07/16/2014 - 13:39

The question is a little vague.  Is it a multi-turn absolute encoder, or a single turn absolute feedback device?  Is the motor being driven past the roll-over point?

For single turn feedback devices in an application where the motor will never pass one revolution, you can use homing mode 13.  This just uses the current position value as the position value and turns on the home done and home found bits.

For mulit-turn absolute encoders in an application where the motor will never pass the multi-turn roll-over point, you don't ever need to run a homing routine.  Just use the FB1.OFFSET parameter to offset the position value to put zero wherever you want it and save it.  You can make a move to zero, but DON'T EVER home it.

For multi-turn absolute encoders in an application where the drive will be rebooted after passing the roll-over point, you must use homing as if the feedback was not absolute.

Lenny Gotham | Mon, 07/16/2018 - 10:48

I'm glad to read this information.
<a href="http://www.markzukcer.com/">Facebook</a&gt;

About this Question

kdn-adm