Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

Stefano Giacomelli's picture
Stefano Giacomelli
3 days 14 hours ago

This example shows how to exchange data between a PCMM or AKD PDMM and a PC using UDP.

The attached KAS program works with the target controller and 2 AKD drives. 

The PC-based program is written in C# and receives the axis positions from the controller. It is also possible to send text to the PC.

Joe Parks's picture
Joe Parks
4 days 6 hours ago

Kollmorgen Visualization Builder (KVB) software has built in alarm features. Users can easily determine when certain values of tags will raise alarms, how they are displayed on the HMI, how they can be cleared, how users can view a history of past alarms, and if text messages or emails should be sent along with certain alarms. The video embedded below goes through the basics of setting alarms and options for how they are viewed on Kollmorgen AKI HMI panels.

C Wontrop's picture
C Wontrop
1 week 3 days ago

This video demonstrates:

  • Backing up a KAS system to the Controller’s SD card
  • Exporting this backup to one system  file on a PC
  • Importing a system file and converting back to multiple files on the SD card
  • Restoring the system configuration from the SD card to the KAS System hardware

Backing Up and Restoring a KAS system facilitates:

Giuliano Comparotto's picture
Giuliano Comparotto
1 week 3 days ago

Válido para S300, S700

Dependendo do problema atual, as falhas são gerenciadas de forma diferente (diferentes níveis de erro):