Back to top

Heat Dissipation Of AKD Drives During The Operation

0 votes
+ vote
Vote up!

Hi! 

I would like to estimate how much heat (in Watt) is generated by the motor drives during their operation. 

The drives that I am using are: AKD-P00306-NBCN-0000 and AKD-P00606-NBCN-0000

Thanks for your help!

0 Comments

1 Answer

0 votes
+ vote
Vote up!

Hi Bing,

The drive losses depend on the drive electronic and the power stage, therefore the power supplied to the motor. This values can be found in the installation manual chapter 7.x Electrical data.

https://www.kollmorgen.com/sites/default/files/public_downloads/AKD_Installation_en_Rev-AB.pdf

For a AKD-P00306/AKD-P00606 it's 31W / 57W @ rated current, where up to 20W will be losses if the power stage is disabled.

Regards,

Martin

Comments

Thank you very much! Super helpful!

Bing - Mon, 06/24/2019 - 09:27
Log in or register to post comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.