Back to top

Function on Digital Out for AKD

Hello,

On the Servostar family, it was possible to assign a function Absolute current value greater than X (or Absolute current value less than X).

This function is not possible on AKD-P drives.

It will be nice to have such a function in some case when we need to replace a Servostar drive with AKD.

Best regards.

Comments

C Wontrop's picture
C Wontrop
Thank you for the feedback. Please note the new AKD2G drive has the option to set a digital output when the current command is  > a preset value. Also in the AKDT and AKDM versions can be written for this task.
C Wontrop's picture
C Wontrop
Thank you for the feedback. The AKD2G has the capability to set a digital output when the current command is greater than a preset level. Also in the AKDT and AKDM versions , code can be written to set a digital output when a preset current level is exceeded.