Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

kenny.hampton@kollmorgen.com's picture
4 days 1 hour ago

Application Note: Using X9 As General I/O

ArielM's picture
ArielM
1 month 2 weeks ago

When configuring the S700 or S300, homing with an absolute encoder you will need to use ROFFSABS. ROFFSABS provides the necessary offset when physically homing. Single Turn Absolute is absolute to 1 rotation of the motor. To home the drive with an absolute encoder, you will want to physically place where 'Home" or Zero might be.

toddevans01's picture
toddevans01
2 months 2 weeks ago

The attached video covers important topics such as ESI (XML)  file acquisition and importation into TwinCAT 3.

Basic setup and motion from the TwinCAT 3 console is also demonstrated.

Finally how to recognize and resolve a mismatch between the Device Description ( ESI ) and the physical AKD2G hardware/firmware revisions when scanning for boxes is covered.

Stefano Giacomelli's picture
Stefano Giacomelli
2 months 3 weeks ago
This solution allows to read the motor positions of three AKD axes using Raspberry HW and Modbus TCP/IP.