Skip to main content

Kollmorgen Support Network

Downloads

Releases for product lines are formatted like "1.x"
Title Release/Version Language Release Date Category All Versions

WorkBench é uma interface gráfica de usuário que permite a configuração de diferentes dispositivos Kollmorgen. Inclui instalador padrão: o aplicativo com arquivos de ajuda completos. O .NET Framework é baixado da Internet, se ainda não estiver instalado. Para obter mais informações sobre os recursos, consulte as notas de versão do AKD WorkBench.

Release: 2.16.0.10498
Portuguese, Brazil Software View all

WorkBench ist eine grafische Benutzeroberfläche, die die Konfiguration von verschiedenen Kollmorgen-Geräten ermöglicht. Enthält Standard-Installer: die Anwendung mit vollständigen Hilfedateien. Das .NET Framework wird aus dem Internet heruntergeladen, falls es noch nicht installiert ist. Weitere Informationen zu den Funktionen finden Sie in den Versionshinweisen von AKD WorkBench.

Release: 2.16.0.10498
German Software View all

WorkBench ist eine grafische Benutzeroberfläche, die die Konfiguration von verschiedenen Kollmorgen-Geräten ermöglicht. Enthält Standard-Installer: die Anwendung mit vollständigen Hilfedateien. Das .NET Framework wird aus dem Internet heruntergeladen, falls es noch nicht installiert ist. Weitere Informationen zu den Funktionen finden Sie in den Versionshinweisen von AKD WorkBench.

Release: 2.16.0.10498
German Software View all

WorkBench 是一个图形用户界面,允许从不同的 Kollmorgen 设备进行配置。 包括标准安装程序:具有完整帮助文件的应用程序。 如果尚未安装 .NET Framework,则从 Internet 下载。 有关功能的更多信息,请参阅 AKD WorkBench 发行说明。

Release: 2.16.0.10498
Chinese, Simplified Software View all

WorkBench 是一个图形用户界面,允许从不同的 Kollmorgen 设备进行配置。 包括标准安装程序:具有完整帮助文件的应用程序。 如果尚未安装 .NET Framework,则从 Internet 下载。 有关功能的更多信息,请参阅 AKD WorkBench 发行说明。

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. For more information regarding features, see the AKD WorkBench Release Notes.

Release: 2.16.0.10498
Chinese, Simplified Software View all

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

Release: 2.16.0.10497
English Software View all

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD Workbench Release Notes. English-only GUI.

Release: 2.16.0.10497
English Software View all

Certificate of Compliance for the P80360 R4E ECE with ISO 13849-1 ISO 13849-2. Safe Torque Off (STO) function, complies with the requirements for PL e, Category 4. 

English Certifications View all

UL Certificate of Compliance for T014-000X, ZMP-SYNQNET-PCI, T015-000X, T115-000X, T114-000X, T127-000X, T131-XXXX and T133-XXXX, T134-XXXX, T135-XXXX Motion Controller PCI Cards. 

Release: 07/2024
English Certifications View all

Certificate of compliance with UL for S20250, S20260, S20350, S20360, S20660 followed by suffixes

Release: 07/2024
English Certifications View all

Certificate of compliance with UL for AKD2G-S-x drives with x=N, C, Q, E, L, P, I, Y, O, or T.

Release: 07/2024
English Certifications View all

Certificate of compliance with UL for AKD-x04807 drives with x=B, P, T, M

Release: 07/2024
English Certifications View all

EU Declarationof Conformity for Goldine ATEX devices. The device conforms to EN 60079-0:2018, EN 60079-1:2014, and EN 61800-3: 2004/A1:2012.

Release: 07/2024
English Certifications View all

Kollmorgen Studio is a software program used for the configuration and diagnostic of Kollmorgen stepper drives. Studio simplifies the process of setting all the operating parameters for the drives and application. The software integrates a digital oscilloscope, allowing you to monitor and instantaneously sample parameters of the motion profile used in motor control. Studio also has functionality dedicated to DS402 profiles and related functions.

Release: 2.0.8
English Software View all

Full setup file for the Kollmorgen Space GUI programming software for the stepper drive P80360

Release: 4.0.2
English Software View all

The PCMM2G controller uses a Kollmorgen customized version of the U-Boot boot loader. 
The contents of this .ZIP file are used to update the PCMM2G's boot loader from the Web server interface.
 

Release: 2022.01.09
English Firmware View all

Used to backup the network topology, the AKD2G drives firmware, and the AKD2G drive's data.

Release: 02-13-00-000
English Firmware View all

File Contents

This .ZIP file contains the PCMM2G's OS build source scripts.

Usage

This .ZIP file is used to build the PCMM2G's OS image.

Note: See the README.md file in the .ZIP file for build instructions and details about what is included in the OS image.

Release: 1.0.0.00407
English Firmware View all

File Contents

This .BZ2 file contains the factory default OS and the RT files.

Usage

  • The contents of this .BZ2 file are used to rebuild the PCMM2G when the main flash becomes corrupted.
  • Customers flash this .BZ2 file onto a PCMM2G and use it to recover their broken PCMM2G. 
Release: OS-1.0.0.00407-RT-4.02.0.94896
English Firmware View all

File Contents

This .ZIP file contains the PCMM2G's OS and RT files.

Usage

The contents of this .ZIP file are used to update the PCMM2G from the web server interface.

Release: 4.02.0.94896
English Firmware View all