Skip to main content

Kollmorgen Support Network

Downloads

Releases for product lines are formatted like "1.x"
Title Release/Version Language Release Date Category All Versions

Complete package of required components for safety-certified use. The package contains firmware, software, support files, and documentation. This package is for SMM1 only. The specific versions of firmware (2.10.00.104), SMM (01.04), and WorkBench (2.13.0.9674) must be used together to be safety certified. The documentation applies to this version specifically. This download includes WorkBench in English, German, and Portuguese.

Release: 1.04
English, German, Portuguese, Brazil Firmware, Software View all

Describes the product life cycle handling for the device. Includes product safety, transport, packaging, storage, installation, decommissioning, maintenance, disassembly, repair and disposal. 

Release: F
English, Spanish, French, German, Italian, Portuguese, Brazil, Chinese, Simplified Documentation View all

Complete package of required components for safety-certified use. The package contains firmware, software, support files, and documentation. This package is for SMM2 only. The specific versions of firmware (2.12.00.105), SMM (02.07.000), and WorkBench (2.15.0.10823) must be used together to be safety certified. The documentation applies to this version specifically.

Release: 2
English Firmware, Software View all

* This version is Safety Certified for AKD2Gs using FS2 or FS3 * * Pair with firmware v02-12-00-105 * WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD and AKD2G devices. For more information regarding features, see the AKD WorkBench Release Notes. This release introduces SMM 2

Release: 2.15.0.10823
English Software View all

* This version is Safety Certified* * Pair with WorkBench v02.15.0.10823 * AKD2G Servo Drive Firmware for EtherCAT, Profinet, Analog, and CANopen for Functional Safety 2 and Functional Safety 3. This firmware complies with recently revised U.S. and E.U. export regulations (E.U. Dual-Use Regulation 428/2009, and U.S. Dual-use regulation EAR Category 3 under ECCN3A225). This release introduces SMM 2.

Release: 02-12-00-105
English Firmware View all

Installation manual for AKD2G drives. Describes the AKD2G series of digital drives and includes mechanical, electrical, software, and functional safety option 3: STO, SS1, SS2, SOS, SLA, SLI, SLP, SLS, SDI, SAR, SSR, SSM, SCA, SBC, SDB, SBT - SIL3, FSoE.

Release: E
English Documentation View all

Installation manual for AKD2G drives. Describes the AKD2G series of digital drives and includes mechanical, electrical, software, and functional safety option 2: SS1, STO, SBC, SBT - SIL3, FSoE.

Release: E
English Documentation View all

TÜV NORD safety certificate declaring the AKD2G (FS1, FS2, FS3) meets the listed safety requirements. Version 2.0 valid until 2025-01-29.

Release: 2.0
English Certifications View all

WorkBench es una interfaz gráfica de usuario que permite la configuración desde diferentes dispositivos Kollmorgen. Incluye instalador estándar: la aplicación con archivos de ayuda completos. El .NET Framework se descarga de Internet si aún no está instalado. Para obtener más información sobre las funciones, consulte las Notas de la versión de AKD WorkBench.

Release: 2.17.0.10920
Spanish Software View all

WorkBench es una interfaz gráfica de usuario que permite la configuración desde diferentes dispositivos Kollmorgen. Incluye instalador estándar: la aplicación con archivos de ayuda completos. El .NET Framework se descarga de Internet si aún no está instalado. Para obtener más información sobre las funciones, consulte las Notas de la versión de AKD WorkBench.

Release: 2.17.0.10920
Spanish Software View all

Kollmorgen WorkBench 2.17.0.10919 Full Setup Portuguese.exe

Release: 2.17.0.10919
Portuguese, Brazil Software View all

WorkBench é uma interface gráfica de usuário que permite a configuração de diferentes dispositivos Kollmorgen. Inclui instalador padrão: o aplicativo com arquivos de ajuda completos. O .NET Framework é baixado da Internet, se ainda não estiver instalado. Para obter mais informações sobre os recursos, consulte as notas de versão do AKD WorkBench.

Release: 2.17.0.10919
Portuguese, Brazil Software View all

WorkBench ist eine grafische Benutzeroberfläche, die die Konfiguration von verschiedenen Kollmorgen-Geräten ermöglicht. Enthält Standard-Installer: die Anwendung mit vollständigen Hilfedateien. Das .NET Framework wird aus dem Internet heruntergeladen, falls es noch nicht installiert ist. Weitere Informationen zu den Funktionen finden Sie in den Versionshinweisen von AKD WorkBench.

Release: 2.17.0.10919
German Software View all

WorkBench ist eine grafische Benutzeroberfläche, die die Konfiguration von verschiedenen Kollmorgen-Geräten ermöglicht. Enthält Standard-Installer: die Anwendung mit vollständigen Hilfedateien. Das .NET Framework wird aus dem Internet heruntergeladen, falls es noch nicht installiert ist. Weitere Informationen zu den Funktionen finden Sie in den Versionshinweisen von AKD WorkBench.

Release: 2.17.0.10919
German Software View all

WorkBench 是一个图形用户界面,允许从不同的 Kollmorgen 设备进行配置。 包括标准安装程序:具有完整帮助文件的应用程序。 如果尚未安装 .NET Framework,则从 Internet 下载。 有关功能的更多信息,请参阅 AKD WorkBench 发行说明。

Release: 2.17.0.10920
Chinese, Simplified Software View all

WorkBench 是一个图形用户界面,允许从不同的 Kollmorgen 设备进行配置。 包括标准安装程序:具有完整帮助文件的应用程序。 如果尚未安装 .NET Framework,则从 Internet 下载。 有关功能的更多信息,请参阅 AKD WorkBench 发行说明。

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. For more information regarding features, see the AKD WorkBench Release Notes.

Release: 2.17.0.10920
Chinese, Simplified Software View all

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

Release: 2.17.0.10918
English Software View all

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD Workbench Release Notes. English-only GUI.

Release: 2.17.0.10918
English Software View all

Used to backup the network topology, the AKD2G drives firmware, and the AKD2G drive's data.

Release: 02-14-00-000
English Firmware View all

This release includes support for SFD-M feedback and addresses several bug fixes. 

Release: 02.14.00.000
English Firmware View all