Back to top
Title Language File Type: Size Release Date
zip S300 / S400 / S600 / S700 Firmware Upgrade Tool
DotNet from 3.5 required.
Release: 3.2.9
English zip 195.16 KB 6/1/16
zip S300 / S700 Firmware Upgrade Tool v.3.15
Upgrade Tool v.3.15 for loading firmware into S300 / S400 / S600 / S700.
Release: 3.15
English zip 194.37 KB 9/15/15
zip S300-S700 Upgrade_Tool (DotNet3.5 Required) (REV 3.1.5).zip
S300-S700 upgrade tool.
Release: 3.1.5
English zip 194.5 KB 1/8/15
zip S300 / S400 / S600 / S700 Firmware Upgrade Tool USB-CAN
Upgrade Tool PCAN_USB S300/400/600/700 USB port and CAN bus 2014: Mit einem aktuellen Betriebssystemen (Windows Vista/7/8) funktioniert die installierte DLL des USB CAN-Dongles nicht mehr. Wenn die Fehlermeldung ILLHW (illegal hardware) erscheint, ersetzen Sie nach der Installation die Datei PCAN_USB.dll im Installationsverzeichnis C:/Programme/Drive Download Utility–USB mit der gleichnamigen einzelnen Datei PCAN_USB.dll aus dem heruntergeladenen ZIP Archiv. 2014: The latest OS systems (WINDOWS Vista/7/8) do not support the standard USB CAN-Dongle DLL file. If the error message ILLHW (illegal hardware) appears, then, after installation, replace the file PCAN_USB.dll in the install folder C:/Programs/Drive Download Utility–USB with the separate file PCAN_USB.dll from the downloaded zip archive.
Release: 2.16a
English zip 412.68 KB 1/2/14
zip S300 / S400 / S600 / S700 Firmware Upgrade Tool Serial Only
DriveDownloadUtility.exe is used for downloading firmware to the S600, S400, and S300 drives. Version 2.16a Serial Only is the best version to use for the S600 drive. Instructions included in the zip file. For the S300 and S700 drives, the newer "Upgrade Tool" is better.
Release: 2.16a
English zip 256.09 KB 9/26/06
zip S300 / S400 / S600 / S700 Firmware Upgrade Tool LPT-CAN
Upgrade tool for S300, S400, S600, and S700 drives LPT-CAN. Parallel port and CAN bus.
Release: 2.16a
English zip 343.94 KB 9/1/06