Back to top
Title Language File Type: Size Release Date
pdf KAS IDE PLC Library Reference Manual EN (REV T)
A technical reference that covers PLC Programming languages. Includes syntax, structure, declarations, programming features, standard blocks, and advanced operations. For software version 3.06.
Release: 3.06
English pdf 2.43 MB 6/21/21
pdf KAS IDE 30 Minutes to Motion EN (REV T)
A quick tutorial to familiarize you with the KAS IDE, basic principles, and the way the program works by creating a simple motion application project. For software version 3.06.
Release: 3.06
English pdf 737.01 KB 6/21/21
pdf KAS IDE User Manual EN (REV T)
Describes the KAS Integrated Development Environment software (KAS IDE). Provides an introduction to key features and implementations, an overview of motion and bus concepts, creating projects, using KAS Simulator and AKD PDMM, KAS tools, coordinated motion, breakdown of graphical interface, reference of available hardware and documentation, and troubleshooting. For software version 3.06.
Release: 3.06
English pdf 31.73 MB 6/21/21
pdf KAS IDE Getting Started EN (REV T)
Quick setup guide that describes system overview and installation of the KAS IDE, KAS Runtime, KAS hardware components, Kollmorgen Visualization Builder, updating firmware, and troubleshooting tips. For software version 3.06.
Release: 3.06
English pdf 2.58 MB 6/21/21
pdf KAS Release Notes EN (REV P)
Describes changes for the KAS IDE software. Includes firmware, software, and hardware system requirements, and an overview of new features, what's changed, what's fixed, and known issues. For software version 3.06.
Release: 3.06
English pdf 623.6 KB 6/21/21
pdf ZMP REACH SVHC Certificate of Compliance
ZMP REACH SVHC certificate of compliance. Specifies substances of very high concern with regards to regulation (EC) No 1907/2006 of the European parliament and REACH Art. 33(1).
Release: 06/21/2021
English pdf 66.15 KB 6/21/21
pdf KAS IDE Motion Library Reference Manual EN (REV T)
A technical reference that covers the EtherCAT Library, System Library, Pipe Network, and PLCopen Motion Library. For software version 3.06.
Release: 3.06
English pdf 11.26 MB 6/21/21
zip KVB 2.40 SP3 Sample Project for AKI2G Panel and AKD2G Motion Tasking
Valid for KVB software 2.40 SP3 Build 2.43.17.0. This HMI program is set up to run motion tasks in the AKD2G drive. The operator can select from 5 motion tasks saved in the drive and run the selected task. The distance and speed of one other task can be edited by the operator. This program is also set up to run a manual jog move in velocity mode. For more information, see the application notes included in this package.
Release: 2.43
English zip 1.14 MB 6/18/21
pdf AKT2G I/O Manual EN (REV B)
This manual provides technical data, installation, and operating instructions for Kollmorgen AKT2G I/O slice devices, including Safety devices. Devices include: AKT2G-AN-240-000, AKT2G-AN-400-000, AKT2G-AN-430-000, AKT2G-AT-410-000, AKT2G-AT-425-000, AKT2G-DN-002-000, AKT2G-DN-008-000, AKT2G-DNH-008-000, AKT2G-DT-008-000, AKT2G-ECT-000-000, AKT2G-EM-000-000, AKT2G-ENC-180-000, AKT2G-ENC-190-000, AKT2G-PSF-024-000, AKT2G-SDI-004-000, and AKT2G-SDO-004-000
Release: 3.06
English pdf 10.94 MB 6/18/21
zip KVB 2.40 SP3 Sample Project for AKI2G Panel and AKD Motion Tasking
Valid for KVB software 2.40 SP3 Build 2.43.17.0. This HMI program is set up to run motion tasks in the AKD drive. The operator can select from 5 motion tasks saved in the drive and run the selected task. The distance and speed of one other task can be edited by the operator. This program is also set up to run a manual jog move in velocity mode. For more information, see the application note included in this package.
Release: 2.43
English zip 446.87 KB 6/18/21
zip KVB 2.40 SP3 Sample Project for AKI2G Panel and AKD BASIC
Valid for KVB software 2.40 SP3 Build 2.43.17.0. An HMI program that is setup to work with a Basic program in the AKD Basic drive. Allows the operator to select and execute five pre-programmed position moves saved in the Basic program. The operator can edit the distance and speed of one pre-programmed position move. Indicators show the status of motion. The HMI will indicate if homing is complete and the homing move can be started from the HMI. See the application note and Basic program in this package.
Release: 2.43
English zip 391.88 KB 6/18/21
pdf QMP REACH SVHC Certificate of Compliance
QMP REACH SVHC certificate of compliance. Specifies substances of very high concern with regards to regulation (EC) No 1907/2006 of the European parliament and REACH Art. 33(1).
Release: 06/11/2021
English pdf 54.97 KB 6/15/21
pdf QMP EU RoHS Declaration (RoHS10)
EU RoHS declaration for all standard AK models in accordance with directive 2011/65/EU and EU 2015/863 of the European parliament.
Release: 06/11/2021
English pdf 70.14 KB 6/15/21
null AKD2G Firmware Release Notes EN (REV 02.07.00.001)
These release notes for the AKD2G drive firmware (software that executes inside the AKD2G drive) describes the changes between the previous firmware releases and the current release. Includes known issues, new features, feature changes, and fixed bugs.
Release: 02.07.00.001
English null 6/11/21
zip AKD Servoverstärker Drive WorkBench GUI Full Setup DE (Rev 2.9.0.6662)
WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. For more information regarding features, see the AKD WorkBench Release Notes.
Release: 2.9.0.6662
German zip 370.9 MB 6/11/21
zip AKD2G Servo Drive Firmware FS1 (AKD2G-S-A-02-07-00-001)
AKD2G Servo Drive Firmware for EtherCAT, Profinet, Analog, and CANopen. This firmware complies with recently revised U.S. and E.U. export regulations (E.U. Dual-Use Regulation 428/2009, and U.S. Dual-use regulation EAR Category 3 under ECCN3A225).
Release: 02.07.00.001
English zip 19.69 MB 6/11/21
zip AKD Servoverstärker WorkBench GUI Standard Setup DE (Rev 2.9.0.6222)
WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.
Release: 2.9.0.6222
German zip 234.67 MB 6/11/21
tgz AKD2G-Firmware-for-KAS-V02-07-00-001
Used to backup the network topology, the AKD2G drives firmware and the AKD2G drive's data.
Release: 02.07.00.001, 3.06
English tgz 4.71 MB 6/11/21
zip AKD Servo Drive WorkBench GUI Full Setup EN (REV 2.9.0.6662)
WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. For more information regarding features, see the AKD Workbench Release Notes.
Release: 2.9.0.6662
English zip 339.2 MB 6/11/21
zip AKD Servo Drive WorkBench GUI Full Setup PT (REV 2.9.0.6222)
WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. For more information regarding features, see the AKD WorkBench Release Notes.
Release: 2.9.0.6222
Portuguese, Brazil zip 374.42 MB 6/11/21
zip AKD Servo Drive WorkBench GUI Standard Setup EN (REV 2.9.0.6662)
WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.
Release: 2.9.0.6662
English zip 339.2 MB 6/11/21
zip AKD Servo Drive WorkBench GUI Standard Setup PT (REV 2.9.0.6222)
WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.
Release: 2.9.0.6222
Portuguese, Brazil zip 238.19 MB 6/11/21
pdf 科尔摩根AKM电机cUL认证
科尔摩根AKM电机cUL认证
Release: 2021
Chinese, Simplified pdf 519.61 KB 6/2/21
pdf 科尔摩根AKM电机UL认证
科尔摩根AKM电机UL认证
Release: 2021
Chinese, Simplified pdf 815.78 KB 6/2/21
pdf AKD2G Installation Manual with FS2 EN (REV A)
Installation manual for AKD2G drives. Describes the AKD2G series of digital drives and includes mechanical, electrical, software, and functional safety option 2: SS1, STO, SBC, SBT - SIL3, FSoE.
Release: A
English pdf 19.83 MB 6/2/21

Pages