Back to top

Download Files from Controller

0 votes
+ vote
Vote up!

Hi,

I need to transfer my files, that I create during program execution, from AKD controller to my computer via network. I tried with ssh but I couldn't complete my task. Which is the ideal way to retrieve files from controller storage?

Regards

Comments

AKD controller is too vague of a description to be able to assist. Can you provide the complete part number of your hardware set? What software are you using?

toddevans01 - Tue, 01/29/2019 - 06:15

I'm sorry
Model number: AKC-PCM-M1-120-00N-00-000
I used WinSCP to download my files from the controller and failed.

xenofontas - Tue, 01/29/2019 - 07:34
Log in or register to post comments

3 Answers

0 votes
+ vote
Vote up!

One option would be to acquire a compatible SD card and backup and restore that way.

Another option would be to use the Webserver to perform file management.

We have no experience using 3rd party file transfer methods such as your examples ( WinSCP etc. ) for performing file management with the PDMM or PCMM.

0 Comments

0 votes
+ vote
Vote up!

The end user is not going to have the KAS IDE installed in his/her computer.

So, I'm searching for a more universal solution.

0 Comments

0 votes
+ vote
Vote up!
Is there a reason you are not using the KAS ( Kollmorgen Automation Suite ) IDE to do archive files to the PC?
0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.