Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

C Wontrop's picture
C Wontrop
3 weeks 6 days ago

The AKD-PDMM controller/drive, PCMM standalone controller, AKD, AKD2G, and S700 drives all contain hardware I/O that can be used in an application to interface to other control elements on the machine. Typically, to minimize overall system cost, IO point on these products are used first before the AKT2G Remote I/O is incorporated. AKT2G Remote I/O will also be used if a signal type not supported by these products is needed in the application (Example: Thermocouple Module). This lesson reviews how to put together a remote AKT2G Remote I/O Block.

toddevans01's picture
toddevans01
1 month 3 weeks ago

We have not tested Omron PLCs with the AKD Ethernet IP drive but have learned a few nuances from supporting customers.

jeeva's picture
jeeva
2 months 1 week ago

This article shows how to make a simple safety Application with KAS and SafePLC2.

The Functional Safety parameters can be configured in WorkBench or in the BBH SafePLC2. Both methods are described here.

kenny.hampton@kollmorgen.com's picture
2 months 3 weeks ago

A description of the thermal sensor options for the AKM2G Standard and Low Voltage series motors.