Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

toddevans01's picture
toddevans01
1 week 4 hours ago
This catalog covers the KM06, KM09, KM11, MH172, MX09, and MX11 series step motors.
JohnKeesee's picture
JohnKeesee
1 month 6 days ago

Sealing is an important design tool used to prolong the life of motors against harsh environments containing dust or liquid contaminants. There are arguably an unlimited number of applications for servo motors and each comes with its own environmental challenges.

Sealing can be compromised or degraded by incorrect applications, harsh conditions or conditions not covered by the design intent.  Even long operating periods under normal conditions will degrade sealing.

toddevans01's picture
toddevans01
1 month 1 week ago

Important to note is that the Import Project feature in KVB is for Exter panel based Information Designer project migration to KVB.  If the HMI project was done with Cimrex panels the migration is two stepped where you need to first update the Cimrex Prog project to Information Designer and then next to KVB.

 

Giuliano Comparotto's picture
Giuliano Comparotto
1 month 2 weeks ago

Nesse artigo abordaremos sobre como utilizar o osciloscópio presente no KAS e como realizar medições em posicionamentos.