Skip to main content

Kollmorgen Support Network

Kollmorgen Automation and Motion Control - Full line catalog

Kollmorgen Full-line Catalog >

At Kollmorgen, we know that OEM engineers can achieve a lot more when obstacles aren’t in the way. With direct sales, engineering support, manufacturing facilities, and distributors spanning the Americas, Europe, the Middle East, and Asia, we’re…
 The Difference Between Continuous Ratings and Holding Continuous Loads

The Difference Between Continuous Ratings and Holding Continuous Loads >

When correctly sizing AC servo motors, it’s important to avoid miscommunication issues. Learn the critical terminology around sizing that leads to safe, reliable operation.

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.

Trade Compliance >

Kollmorgen is committed to sourcing components and materials from companies that share our values regarding respect for human rights, integrity and environmental responsibility. Kollmorgen is also committed to complying with Section 1502, in…

Can You Integrate a Superior Motor into Your Existing Food and Beverage Production Line? >

Every machine designer wants to deliver the best possible performance. Especially in today’s food and beverage industry, the pressure for optimum throughput and quality means that every OEM is striving to engineer new systems that are the best of the…

Resolving Servo Feedback Choices >

This PowerPoint presentation explains the differences between different types of servo motor feedback devices, including: The differences between absolute and incremental devices. The differences between analog and digital devices. Typical…
AKM Washdown transparent

AKM Washdown and Food Grade >

AKM Washdown and Washdown Food Series servomotors incorporate a protective 2-K coating, IP67-rated seals, stainless steel hardware, special greases and other materials designed for applications such as food, beverage and pharmaceutical processing where hygiene and frequent cleaning are critical requirements.

Ingress Protection of Servo Motors >

Sealing is an important design tool used to prolong the life of motors against harsh environments containing dust or liquid contaminants. There are arguably an unlimited number of applications for servo motors and each comes with its own…

Kollmorgen Automation Solutions and Product Catalog EMEA >

Kollmorgen Automation and Motion Control Kollmorgen: Your partner. In Motion. Every solution comes from a real understanding of the challenges facing machine designers and users.
Subscribe to AKM Washdown