profiles creation
get error 102 on MLPROFILEBUILD is use anything other then zero for camprops.InputOffset.
Thought this was just like a master start offset?
Kollmorgen Support Network
To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.
Please submit your question using the contact us form to reach our application engineering team.
For the immediate future, you can still access and read past posts.
Thank you for understanding and for participating in the community over the years.
get error 102 on MLPROFILEBUILD is use anything other then zero for camprops.InputOffset.
Thought this was just like a master start offset?
MLProfileBuild Error
Description of error 102 is "Element master or slave position is outside the range defined by Cam_Props"
Since the issue is when you try to change the InputOffset to a nonzero value, does the first input or master point start at this same value? Also, does this value cause any master points to be less than the entered value? For example, if input offset is set to 3 and you have some points with a value of 0 you could get the error. I recommend setting the value to the same as the first profile points master position.