Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

MOTOR.TEMPC and Modbus | 02 Jun 2023 | |

MOTOR.TEMPC and Modbus

Is it possible to read by Modbus the motor temp (in case of KTY obviously) through MOTOR.TEMPC ?

I find the register address for MOTOR.TEMP (in ohm), but not MOTOR.TEMPC

 

Best regards

Comments & Answers

Joerg Muslewski | Fri, 06/02/2023 - 11:09

jcoleman02 | Fri, 06/02/2023 - 12:29

Although MOTOR.TEMPC is a 16bit parameter, it has two 16bit registers.  1800 is the upper and 1801 is the lower.  You can read both as 32bit or read 1801 as 16bit.  The value of register 1800 will always be zero.

About this Question

defty
Taxonomy: