Skip to main content

Kollmorgen Support Network

Motor Temperature as Analog Output | 03 May 2023 | |

Motor Temperature as Analog Output

I am using an AKD-P01206-NBEC to drive an AKM64K-ANA2GK motor and am wondering if there is anyway to configure the analog output of the AKD drive to output a signal relative to the motors temperature. 

Comments & Answers

jcoleman02 | Wed, 05/03/2023 - 13:58

No.  Motor temperature is not a selectable function for the AKD drive's analog output.  You can see the allowable selections in the Workbench analog output screen or in the help documentation for AOUT.MODE.

About this Question

Gabriel Knight
Taxonomy: