Back to top

Change me ServoStar drive

0 votes
+ vote
Vote up!

Hi,

I have a servostar drive CR10250-000000  withe M-403-B-A2. i would like to change my drive to AKM bute the broblem it's a bout cable to motor.

My first question : witch drive can i use To change my old one!

Second question: is there any adapter to connect my encoder to the drive!

i can't find the Datasheet for CR1025 do you have a link to download!

thank you 

0 Comments

1 Answer

0 votes
+ vote
Vote up!

Hello,

The  B-403-B has a continuous current rating of 6.4 Arms, so you should select a AKD-x01206-NBAN-0000 drive.  We do not sell an adapter to convert the feedback cable from CD to AKD connection.

I have attached couple of li The  B-403-B has a continuous current rating of 6.4 Arms, so you will select a AKD-x01206-NBAN-0000 drive.  

https://www.kollmorgen.com/en-us/developer-network/goldline-motor-configuration-akd/

https://www.kollmorgen.com/en-us/developer-network/akd-series-drive-connections-goldline-series-motors/

https://www.kollmorgen.com/en-us/products/brochures/akd-scalability-brochure-en/

Please contact our Applications Group Level 1 directly if you need help more help selecting the AKD drive.

North America

Kollmorgen

203A West Rock Road
Radford, VA 24141

United States

[email protected]
1-540-633-4152
Fax: 1-540-639-4162

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.