Back to top

Cannot Connect to AKD Drive

0 votes
+ vote
Vote up!
My device is not discoverable. When pressing the network ID button, I get 1P169.254.250.133 in reply. What is the IP address of my Kollmorgen device?
0 Comments

1 Answer

0 votes
+ vote
Vote up!

The IP address of your Kollmorgen device is 169.254.250.133 as shown on the drive display.

Please refer to AKD Online help >>Workbench User Manual > Connecting the AKD<< and >> Workbench User Manual > Communicating with the AKD<< for further details.
http://curvegen.kollmorgen.com/webhelp/workbench/English

If auto-discovery of the Workbench tool (GUI) doesn't, you can enter the shown IP 169.254.250.133 manually and connect to the drive.
Please check the network and firewall settings of your PC as well.

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.