Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

AKM Temperature Feedback | 29 Jul 2015 | |

AKM Temperature Feedback

A customer of ours wants to monitor motor temperature. The motor temperature under properties does not report a valid number. He only sees -32,768 degC as the temperature.

Motor feedback is SFD. Motor autoset is 'ON'.

Thermistor type is the default value 0-Single PTC Thermistor.

These are the motor and drive part numbers:

AKM51L-EKGNC-00

AKD-P01206-NBEI-0000

He bought the drive recently, only one month ago. He is running the latest version of workbench.

I could not get a snapshot email from him because he does not have email setup on his PC.

Maybe I am looking at the wrong parameter value. Please advise. Thanks!

 

Comments & Answers

Joerg Muslewski | Thu, 07/30/2015 - 08:50
The PTC thermistor does not support temperature monitoring in degC. It is a thermistor with a non-linear characteristics.  
To monitor the temperature, your customer needs a motor with an integrated KTY thermistor or you need to use an external device.
Please, refer also to the AKD documentation of parameter <MOTOR.RTYPE>, <MOTOR.TEMP>, <MOTOR.TEMPC>.
Please, get in contact with your local sales representative, if you want to replace the AKM motor by an AKM with integrated KTY.

Ian Johnson | Thu, 07/30/2015 - 19:26
Is there a table of temperature values for the standard PTC thermistor so that he can map the resistance to temperature externally?

Joerg Muslewski | Tue, 08/04/2015 - 06:19

About this Question

Ian Johnson
Taxonomy: