Back to top

AKD PDMM Communication Error.

0 votes
+ vote
Vote up!

Hi , I am using 

KAS IDE Version: 3. 00 Build 3, 00, 0, 75985.

AKD-M-MCEC-V01-17-00-000

KAS-PDMM-M-MCEC-3.00.0.75985

 I connect AKD with S7 315 PLC.  Initially after i download the program, PLC  PLC shown the AKD device connection not stable.

afterward i try to increase the update time to 8 ms and  watchdog to 7 cycle..form TIA portal as this community suggested, it seem the AKD device connection stable from TIA portal view.. 

But form KAS IDE, always there is error message 

7  |  | 16/11/2018 6:16:25 PM (747) | Motion     | ERROR | Received read request with AR UUID {0da920b4-85e9-5c42-896d-b1398b77f9c4}. (Slot 0000., Subslot 0001, Index 800c.), PNIO error de80b000 | T5VirtualMachine.cpp:212 
8  |  | 16/11/2018 6:20:19 PM (314) | Motion     | ERROR | Watchdog for CR {2} in AR {0da920b4-85e9-5c42-896d-b1398b77f9c4} expired. 11 PNRTC frames missing                                       | T5VirtualMachine.cpp:212 
9  |  | 16/11/2018 6:20:32 PM (617) | Motion     | ERROR | Received read request with AR UUID {0da920b4-85e9-5c42-896d-b1398b77f9c4}. (Slot 0000., Subslot 0001, Index 800c.), PNIO error de80b000 | T5VirtualMachine.cpp:212 
10 |  | 16/11/2018 6:20:46 PM (060) | Motion     | ERROR | Received read request with AR UUID {0da920b4-85e9-5c42-896d-b1398b77f9c4}. (Slot 0000., Subslot 0001, Index aff0.), PNIO error de80b000 | T5VirtualMachine.cpp:212 
 

If i disconnect TIA portal online status, the error message stop generated. Should i continue testing to increase the update time Or watchdog time (Which one better) until it stable? what are the advice able setting  limit or there is other special setting i need to take care?

I have another error. message 

   |  | Time                        | Source     | Level | Message                                                                                                                                 | Location                 
---+--+-----------------------------+------------+-------+-----------------------------------------------------------------------------------------------------------------------------------------+--------------------------
1  |  | 16/11/2018 6:16:20 PM (426) | Controller | ERROR | OnBoardIODriver: Another variable is already mapped to IO index 0.                                                                      | OnboardIODriver.cpp:125  
2  |  | 16/11/2018 6:16:20 PM (426) | Motion     | ERROR | Variable 'X7_MANUALHOMING' IO '%IX0.0.0.0' creation failed (at driver level)                                                            | T5VirtualMachine.cpp:2964
3  |  | 16/11/2018 6:16:20 PM (426) | Controller | ERROR | OnBoardIODriver: Another variable is already mapped to IO index 0.                                                                      | OnboardIODriver.cpp:125  
4  |  | 16/11/2018 6:16:20 PM (426) | Motion     | ERROR | Variable 'X7_MANUALCRASHNHOLD' IO '%IX0.0.0.0' creation failed (at driver level)                                                        | T5VirtualMachine.cpp:2964
5  |  | 16/11/2018 6:16:20 PM (426) | Controller | ERROR | OnBoardIODriver: Another variable is already mapped to IO index 1.                                                                      | OnboardIODriver.cpp:125  
6  |  | 16/11/2018 6:16:20 PM (426) | Motion     | ERROR | Variable 'X7_MANUALCRASHNHOLD' IO '%IX0.0.0.1' creation failed (at driver level) 

where can i find this error location and fix it?  i don't knwo where is location to access OnBoardIODriver: Another variable is already mapped to IO index 1.  

Thanks

 

 

0 Comments

1 Answer

0 votes
+ vote
Vote up!
Sample communication program provided to the customer on 11/19/2018 by Gavin W.
0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.