Back to top

AKD EthernetIP communication with Omron PLC problem

0 votes
+ vote
Vote up!

When import EIP.EDS file to Omron PLC, the PLC output start address is D200, input start address is D100, and Ethernet_IP manual did not tell us the sequence of

control , what's the right code of Position mode and Jog mode?

0 Comments

1 Answer

0 votes
+ vote
Vote up!

We are not familiar with programming an Omron PLC.  The Omron people have written a user manual for setup and operation of the AKD and Omron PLC.  I do know the Omron and AKD will only work in Cyclic Synchronlusposition mode.  Jogging motion profile will have to be 100% generated in the PLC.

Comments

where can i find the last revicion of Ethernet IP EDS File to AKD?? do you have some example of connexion with omron??

Daniel_Barmex - Wed, 08/12/2015 - 13:50
Log in or register to post comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.