Back to top

AKD DRIVES

0 votes
+ vote
Vote up!

Hi there.

 

I have one of the akd control systems, used for controlling PET blowing machine. the system has a fault which is 418 primary feedback power supply fault, I traced the pins of the power supply, according to the manual it should be 5 volts , but on mine it is 1.2 volts which is not enough to supply the encoder, I do not know what caused this fault. 

help is highly appreciated.

0 Comments

5 Answers

0 votes
+ vote
Vote up!
image

Comments

Hi again.
After checking the cable and the encoder I reached out that the drive is the faulty one, what I concerned about is that what could cause this fault because it happened to three of our drives including the controller.
hope can help

tahnk you

Rafiq

Rafeq - Tue, 01/18/2022 - 01:01
Log in or register to post comments

0 votes
+ vote
Vote up!
image
0 Comments

0 votes
+ vote
Vote up!

Check your external 24 volts logic supply that's connected to the AKD drive, connect X1 to make sure it is at level of 24 volt dc. There could be an issue with the feedback cable you are using, the Endat encoder, or the AKD drive.

I would check your feedback cable first.  If you give me the motor model no. I can supple the cable feedback connections.

 

Thanks,

Kenny Hampton 

  

Comments

Hi again.
The motor model is AKM51G ANC2LB

Thank you
Rafiq

Rafeq - Mon, 01/17/2022 - 13:21
Log in or register to post comments

0 votes
+ vote
Vote up!

The  Endat 2.1 output voltage should be 5 volts.

Thanks,

Kenny Hampton

0 Comments

0 votes
+ vote
Vote up!

Hello

The feedback output supply should be around 5 to 8 volts depending on your feedback device.

 

Thanks,

Kenny Hampton

Comments

Thanks Kenny, but what I need to know is that why there is lower voltage than it should be although the feedback type selected properly which is EnDat 2.1

Thanks again.

Rafeq - Mon, 01/17/2022 - 11:48
Log in or register to post comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.