Back to top

AKD does not move after SetPointAcknowledge - Ethercat

0 votes
+ vote
Vote up!

Hi,

I'm using an instance of IgH Ethercat Master for Linux and we're facing the issue of not having the movement set through registers 0x607A, 0x6081, 0x6083 and 0x6084 - target position, velocity, accel, decel, respectively - executed, even after getting the acknowledge setpoint from bit 12 of StatusWord (0x6041), below is our sequence of operation, considering we already have the device enabled on Profile Position mode:

1 - write position data through 607A, 6081, 6083 & 6084

2 - Start motion with 0x3F in 6040

4 - Wait bit 12 of 6041 = 1

5 - Set 6040 to 0x2F

6 - wait a rising edge transition on bit 10 of 6041 - which means the movement has been finished

7 - eventually the movement does not happen, so execute steps from 2 to 5 again

We've noticed that this happen around 2% of time - most of movements are executed exactly as expected - we try to execute a movement and also noticed that on Workbench there is no warning regarding communication failure registered when this event happens. We are using Trapezoidal Motion Profile and also bit 5 of 0x6040 set just to ensure the movement get start the moment we apply a rising edge on bit 4 of control Word as described on RGM Canopen Manual but the problem is still there.

Has anyone already seem this behavior?

0 Comments

No answers have been submitted for this question.

ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.