Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

AKD Communication issues | 25 Jul 2015 | |

AKD Communication issues

Hi,

I'm using AKD-P00306-NBAN-0000 model and i can't communicate this drive to RS Logix 5000 PLC.could somebody can help me to resolve this issue.

 

Comments & Answers

jcoleman02 | Sat, 07/25/2015 - 20:27
That AKD model does not support Ethernet/IP fieldbus communications. It only supports Telnet and Modbus TCP. If you need Ethernet/IP, then you must use the AKD-P00306-NBEI-0000 drive model.

Murali Sankar … | Sun, 07/26/2015 - 01:39
Ok Thanks !! I have another question that when I'm using an external digital input command for start homing and start motion task.i used DIN 1 and DIN 2 but when i give the command through switch sometimes it is work and sometimes it is not working. My settings, DIN 1 start home para 1 polarity high. And DIN2 start motion task para 1 polarity high These settings which i done on workbench. Servo digital I/O. So please give me some suggestion to resolve it. Thanks, Murali.

Joerg Muslewski | Thu, 07/30/2015 - 09:51
You can record the value of the digital inputs (DIN1.STATE, DIN2.STATE) by workbench scope function when the problem occurs,
in order to exclude possible disturbance of the signals. Might also be a timing problem. The last action ist still in progress when you try to activate the next one.

About this Question

Murali Sankar …
Taxonomy: