Back to top

AKD can bus DINx . STATUS .. can you read the status of the inputs via the can bus.

0 votes
+ vote
Vote up!

Hi again

Can you read the status of the inputs via the can bus?

In the manual is says it is supported but there is no address given.

Does this mean I cant do it or is this bit missing from the manual ?

Thank for any reply

wishing you well

Adam.

0 Comments

1 Answer

1 vote
+ vote
Vote up!

Per the manual (page 173) the DINx.STATE for inputs 1 to 7 can be accessed from the following object.

image

Comments

Thank you.

Adam Phipps - Fri, 01/08/2021 - 01:55
Log in or register to post comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.