Back to top

Add resolver frequency to AKD User Guide

In the next revision of the AKD User Guide (P/N 903-200006-00), add the following note at the end of section 9.3.2.8 Resolver (p.76):

(link to AKD User Guide: http://www.kollmorgen.com/en-us/products/drives/servo/akd/_manuals/kollmorgen-akd-user-guide-en-rev-n/)

(Only the information between the horizontal lines is to be added to User Guide.)


Note.jpg


The manual makes clear that non-Kollmorgen standard resolvers are not supported, but the added note lets those interested know the frequency used, while also stating that it is not customer-settable/changeable.

Comments

dmcleod's picture
dmcleod
Thanks Bill, this will be in the next revision.
Mike_Kilroy's picture
Mike_Kilroy
Why do we make such a BOLD statement that non Kollmorgen resolvers are not supported?  It says now: "Currently, the AKD does not support non-Kollmorgen standard resolver options." Can't it say instead something like: "Although non-Kollmorgen resolvers are not supported, most should work fine." I have many Moog, Allen Bradley, AEG, CSM, Parker, SEM servos running fine with their resolvers on AKD.....