Back to top

KAS/IDE - Add Drag-n-Drop for Program Display Order in Project Explorer

Currently the only way to change the order the programs are displayed is to export them all, delete them all, and then import them in the order you want them displayed.  This is quite cumbersome.

Comments

cwontrop's picture
cwontrop
Which product are you referring to?
BAJ's picture
BAJ
KAS/IDE
cwontrop's picture
cwontrop
That is correct: the only way to change the order the programs are displayed in the KAS IDE is to export them all, delete them all, and then import them in the order you want them displayed. There is a way to change priority of execution as explained here: http://kdn.kollmorgen.com/webhelp/kas/#4.UsingKASIDE/Define scheduling_PLC_cycle.htm