Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

JohnKeesee's picture
JohnKeesee
1 week 4 days ago
Summary of Juran's Mean Time Between Failure (MTBF) for AKD & AKM.  Data up through 2014.
C Wontrop's picture
C Wontrop
2 weeks 6 days ago

AKD-PDMM controller/drive, AKD, AKD2G, and S700 drives, and PCMM standalone controller all contain hardware I/O that can be used in an application to interface to other control elements on the machine. Typically, to minimize overall system cost, IO point on these products are used first before the AKT Remote I/O is incorporated. AKT Remote I/O will also be used if a signal type not supported by Kollmorgen drives and controllers is needed in the application. This lesson reviews how to put together a remote AKT Remote I/O Block.

Stefano Giacomelli's picture
Stefano Giacomelli
1 month 1 day ago

This example shows how to exchange data between a PCMM or AKD PDMM and a PC using UDP.

The attached KAS program works with the target controller and 2 AKD drives. 

The PC-based program is written in C# and receives the axis positions from the controller. It is also possible to send text to the PC.

Joe Parks's picture
Joe Parks
1 month 2 days ago

Kollmorgen Visualization Builder (KVB) software has built in alarm features. Users can easily determine when certain values of tags will raise alarms, how they are displayed on the HMI, how they can be cleared, how users can view a history of past alarms, and if text messages or emails should be sent along with certain alarms. The video embedded below goes through the basics of setting alarms and options for how they are viewed on Kollmorgen AKI HMI panels.