Back to top
04 Apr 2018

Kollmorgen to Exhibit Motion Solutions for Robot Designers & Manufacturers at AUVSI XPONENTIAL 2018

XPOTENTIAL 2018 smRADFORD, VA – April 4, 2018 – Kollmorgen will feature its newest motion solutions for robot design for engineers and manufacturers at the AUVSI XPONENTIAL SHOW, May 1-3, in Denver, CO. Visitors to Booth #4109 can expect to see live product demos and discuss real-world applications with Kollmorgen experts on site.

Kollmorgen’s advanced servo, frameless, and stepper motors deliver the high-power density, optimized packaging, and increased precision critical to building superior robots. Applications include robotic arms and joints, collaborative robots, and medical robots, as well as Automated Guided Vehicles (AGVs) such as mobile picking/sorting robots, carts, tuggers, and self-driving forklifts.

Throughout the show Kollmorgen will highlight its latest brushless and frameless motors including the TBM™ Series. These direct drive frameless motors are ideal for applications that require high power in a compact package with minimized weight and inertia. The configurable nature of the TBM family allows manufacturers to optimize motor selection to match specific requirements for applications.

For more information about Kollmorgen technologies, please visit www.kollmorgen.com, call 540-633-3545, or stop by Booth #4109 during the show.

ABOUT KOLLMORGEN
Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough motion solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind.

For more information visit www.kollmorgen.com, email [email protected]rgen.com, or call 540-633-3545.