Back to top
04 May 2017

KOLLMORGEN expands its AKM servomotor series

Extra-low-voltage motors as a solution for machine modules and retrofitting

Kollmorgen AKM Low Voltage

Ratingen, April 2017 - Energy efficiency, durability, power density, overload capability: KOLLMORGEN has now transferred these four benefits of permanent-field servo motors to the extra low voltage world. The new AKM DC servo motor low voltage with its 48-volt design was originally intended as a customer-specific solution for special areas of use. Kollmorgen – A specialist in servo-drive technology and motion control will now offer this as a standard add-on to the AKM series, and thus as a new series product. There are many potential uses for 48 volt DC servo motor low voltage.The same applies to two new variants with a 24 volt power supply.

Size 3 AKM low voltage servo motors of 48 volts provides up to 300 watts of power at a current of 6 A – sufficient, for example, for accurate drive tasks in packaging machines or for dynamic movement in autonomous transport systems. Because the axes can briefly provide a peak current of up to 15 A, the breakaway torques predominant on start-up are easily overcome, which, at the end of the day, prevents permanent over dimensioning of the drive technology. The static torque is 1.25 Nm with an impulse torque of 4.1 Nm. Further variants of KOLLMORGEN AKM low voltage DC servo motor include two 48 V motors with less power, and two drives with windings tailored to 24 volts.

Thanks to its compact form, the extra low voltage servo-axis can be very easily retrofitted in existing installations and additionally allows space-saving surface mounting of machine modules with autonomous intelligence – in the form of a labeling unit, for example.

Fig. 1 – AKM31S servomotor
Drive solution in the labeling unit of a packaging machine using AKM31S

Fig. 2 – AKM low-voltage servomotor
Extra-low-voltage drive in an autonomous transport system. Autonomous transport systems equipped with extra-low-voltage servo-axes are characterized by their high levels of accuracy and dynamic movement.

Fig. 3.1 + 3.2 – AKM extra-low-voltage servomotor
The AKM motor series provides maximum flexibility for any application

Kollmorgen Press Kit

ABOUT KOLLMORGEN
Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind. For further information please contact [email protected] or visit our website www.kollmorgen.com/uk