Back to top
20 Nov 2015

Double the performance in the field

Ratingen, 20. November 2015 - KOLLMORGEN expands its fields of application for the distributed servo technology with a significant increase in performance. The three-phase AKD-N series now delivers currents up to 12 A – equivalent to a doubling of output to 4.8 kW. The AKD-C central rectifier units are also bringing more power. With 20 kW the compact devices are now also providing double the previous maximum continuous output of 10kW. The short-term peak output for both devices is at just short of three times the nominal current.

With its distributed servo technology in protection class IP67, AKD-N enables KOLLMORGEN to incorporate drive functions on-site in a machine. This results in smaller switch cabinets, better options for modularization, drastically reduced cabling outlay, and greater flexibility in construction. The AKD-N servo system from KOLLMORGEN therefore also supports fast and cost-efficient installation using single-cable connection technology and options to use the devices in conjunction with Ethercat for collecting I/O signals.

Kollmorgen Press Kit

Caption 1
KOLLMORGEN has doubled the performance range of its distributed AKD-N servo drive control system to 12 A.

ABOUT KOLLMORGEN
KOLLMORGEN is a leading provider of integrated automation and drive systems and components for machine builders around the globe. With over 70 years of motion control design and application expertise and deep expertise in constructing standard and custom solutions, KOLLMORGEN always delivers solutions which are characterized by performance, quality, reliability, and ease-of-use. Customers can therefore gain an irrefutable marketplace advantage. – Further information: www.kollmorgen.com | [email protected]

© KOLLMORGEN. Use for editorial purposes free of charge.