Back to top
31 Jul 2014

Tomorrow’s technology must become simpler

PackPlus India: KOLLMORGEN presents a new machine design

Mumbai, 31 July 2014. Solutions that really dispense with everything that is not absolutely necessary – this is what is meant when KOLLMORGEN talks about Simple Machine Design. The experts in servo drive technology and motion control will show at PackPlus South (India) why this new simplicity shines directly on the real spirit of the times for machinery and plant engineering. KOLLMORGEN will prove this statement from 17 to 20 September 2014 during the largest packaging fair, in Hyderabad, India

Preferably maintenance-free, flexible and easy to use. These wishes of the foodstuffs and packaging industry will in future ensure even more that machines are built that have simple modular structures. “Next Gen Machine DesignNow”: KOLLMORGEN will show in Hall 2, on Stand 2.57 just what role drive technology plays in the process, amongst other things with the decentralised AKD-N servo drive series.
These robust devices can, thanks to their compact dimensions and high degree of protection, be integrated very easily close to the motor in machinery designs. Furthermore, the single cable connection technique with an only eleven millimetre thin hybrid cable between the controller and the motor lowers the installation costs. Together with the high grade steel AKMH servo motors, cleaning the equipment will also become a lot easier.

KOLLMORGEN has honed this trend-setting drive technology in such a way that the centralised and decentralised benefits can be exploited with just a standard cable – irrespective of which motor is just in need of connection to which recovery system. Whether it’s a robust resolver or a high definition multi-turn sensor: in this way KOLLMORGEN lowers the costs of warehousing and variety management. Furthermore, individual drive axles can – for instance during commissioning – be more easily functionally adapted without constant need to also re-lay the cables.

Visit us at PackPlus South and make an appointment now

Kollmorgen Press Kit

Photo Text:
Slimmed down: with its decentralised servo drives and its single cable connection technique, KOLLMORGEN opens new routes to a slim hygienic design for machinery and plant.

About Kollmorgen
Kollmorgen is a leading provider of integrated automation and drive systems along with corresponding components for machine builders all over the world. With more than 70 years of Motion Control Design and application experience and profound knowledge of constructing standard and special solutions, Kollmorgen supplies solutions time and again that stand out in terms of performance, quality, reliability, and ease of use. As a result customers can achieve a market advantage which is beyond question. For further information please contact [email protected] or visit our website www.kollmorgen.com

© Kollmorgen.