Back to top
09 Dec 2014

Quickly Select a Motion Solution Optimized to Suit Specific Application Needs with Kollmorgen's NEW Web-based MOTIONEERING® Online Application Engine

MOTIONEERING Online simplifies the sizing and selection of rotary motor and drive systems to help get better performing machines to market, faster and is available on-line for your convenience!

MOTIONEERING OnlineRADFORD, VA - December 9, 2014 - Kollmorgen introduces a new tool that will provide a better experience in motion system sizing and selecting - MOTIONEERING® Online ( www.kollmorgen.com/motioneering). This premiere OEM design tool utilizes a mechanism project concept to collect and save load information for multiple axes. This design tool automatically calculates application results and compares them against Kollmorgen's robust database of products allowing for quick identification of the optimized rotary motion system to meet specific machine builder application requirements. Similar to our PC-based Motioneering Application Engine, our new online tool features a wide variety of mechanism types to help simplify the tedious task of specifying optimized motors and drive systems.

MOTIONEERING Online ResultsMOTIONEERING Online includes a user-friendly Help System that explains program functions, definition of terms, and algorithms used to perform application results. Versatile units-of-measure options for mechanism and motion profile data-entry, along with the ability to convert data into other available units, make this a convenient tool for international machine designs as well.

Once application results are calculated and system selections are made, the MOTIONEERING Online PDF generator creates a complete report of application results, system and product specifications, and system performance and user-profile curves with application placement within the plot - ready for easy review and distribution.

ABOUT KOLLMORGEN

Kollmorgen is a leading provider of motion systems and components for machine builders around the globe, with over 70 years of motion control design and application expertise.

Through world-class knowledge in motion, industry-leading quality and deep expertise in linking and integrating standard and custom products, Kollmorgen delivers breakthrough solutions unmatched in performance, reliability and ease-of-use, giving machine builders an irrefutable marketplace advantage.

For more information visit www.kollmorgen.com, email support@kollmorgen.com or call 1-540-633-3545.