Back to top
24 Feb 2014

Kollmorgen Stainless Steel AKMH™ Servo Motors Honored as Finalist in the 2013 Design News Golden Mousetrap Awards

AKMH 265x265 Image
Golden Mousetrap award icon

 Robust design raises the standard for hygienic, washdown servo motors and cables for food, beverage, pharma and caustic chemical environments  

RADFORD, VA – Kollmorgen announces that its line of robust stainless steel AKM™ servo motors has been selected as a Golden Mousetrap Finalist in the Automation and Control category. The Awards celebrate the companies, products, and people who are energizing North American design, engineering, and manufacturing. The Golden Mousetrap Awards were announced at the Golden Mousetraps Ceremony held February 11, 2014 at the Anaheim Marriott.

Design News’ industry leading editors worked tirelessly to go through the many entries received to come up with the products most deserving to be on our list of finalists. The finalist entries were then sent to the entire editorial team, as well as our distinguished Advisory Board to choose the winners.

“We are confident that the Kollmorgen AKMH Servo motor is the best-performing and longest-lasting stainless-steel washdown motor in the industry today. These motors combine industry-leading performance and a robust hygienic design to deliver reliable and consistent performance that can be the difference between a commodity product and differentiated machine for OEMs,” says Gene Matthews, Product Manager. “The innovative design of AKMH helps end-users over the long haul by simplifying sanitation requirements and minimizing the potential for contamination. In turn, this helps companies protect their brands by reducing the risk of devastating product recalls.”

Designed specifically to address the Food Safety Modernization Act (FSMA), these IP69K rated synchronous servo motors feature a hygienic housing design that meets EHEDG, NSF, BISSC, USDA and 3A guidelines. The AKMH Servo motor is constructed with materials to provide long-life and trouble-free operation, even with daily exposure to chemicals and high pressure washdowns. AKMH’s single-cable solution reduces the number of potential failure modes and minimizes installation time. The smooth surface design, and use of highly corrosion-resistant 316L stainless steel, decreases the risk of product recalls by reducing the possibility of bacteria growth. The AKMH requires no additional protection and can be sanitized without covering it or removing it from the machine. As a result, food, beverage, packaging, medical, pharmaceutical and converting OEMs can design and build more reliable and productive machines that are easier and faster to clean, thus minimizing unscheduled downtime for end users.

Available as a Complete and Optimized Package

AKMH Servo motors can be combined with an AKD® servo drive or AKD® PDMM for a completely optimized, high performance motion system that delivers a distinct competitive advantage for OEMs, and brings cost savings to end-users through increased reliability and reduced cleaning time. Kollmorgen is so confident in the quality and performance of the AKMH/AKD combination that the company backs it with a two year warranty against water ingress –the best warranty in the industry.

Read about more about the Golden Mousetrap Award Finalists and Winners on designnews.com, Facebook, or Twitter. Images from the ceremony will be posted to the Design News Facebook page.

ABOUT UBM CANNON

UBM Canon is the leading B-to-B event producer, publisher, and digital media company for the world’s $3 trillion advanced, technology-based manufacturing industry. Our print and electronic products deliver trusted information to the advanced manufacturing market and leverage our proprietary 1.3 million name database to connect suppliers with buyers and purchase influencers. We produce more than 50 events and conferences in a dozen countries, connecting manufacturing professionals from around the globe. UBM Canon is part of UBM plc (UBM.L) a global provider of media and information services for professional B-to-B communities and markets.

ABOUT KOLLMORGEN

Kollmorgen is a leading provider of motion systems and components for machine builders around the globe, with over 70 years of motion control design and application expertise. Through world-class knowledge in motion, industry-leading quality and deep expertise in linking and integrating standard and custom products, Kollmorgen delivers breakthrough solutions unmatched in performance, reliability and ease-of-use, giving machine builders an irrefutable marketplace advantage.

For more information visit www.kollmorgen.com, email [email protected] or call 1-540-633-3545.