SPS IPC Drives: “Intelligent Motion” - a key aspect for KOLLMORGEN
Ratingen, 29.10.2014. In the end everything is simple: If primary requirements such as “simple", “efficient” or “connected” are mentioned when equipping a plant, we lose focus on technology in favor of a broader view of things. What can drive and control technology provide here? This is the question that KOLLMORGEN will consider during the SPS IPC Drives Exhibition from 25 to 27 November 2014 in Nuremberg (Hall 3a, Stand 230).
Why go through the controls when you can directly access the controller of the intelligent KOLLMORGEN AKD PDMM servo drive with your tablet or smartphone? This smart way provides further opportunities for the user to run preventive diagnostics on data from drives or motor sensors. In the same way, with this smart method it becomes easier to optimize machine movements and operating robots is child’s play. KOLLMORGEN will show what’s already possible today with “Intelligent Motion” live in action at the 25th SPS IPC Drives Exhibition.
Under the title “Next Gen of Motion Technology – Now”, the specialist in servo drive technology and motion control will also use real exhibits to show the difference between traditional machine automation and the new ways that already allow movements to be generated more intelligently, easily, and efficiently. Machine safety, energy efficiency, intelligent motion sequences, slim designs, highly-integrated functions, gesture-controlled visualization: The list spans all the areas where mechanical engineers and operators develop their requirements of a "Next Gen of Machine Technology”.
Image text:
“Intelligent Motion” - live in action: KOLLMORGEN links servo drive technology with smart devices during SPS IPC Drives.
Photo: Kollmorgen
About Kollmorgen
Kollmorgen is a leading provider of integrated automation and drive systems along with corresponding components for machine builders all over the world. With more than 70 years of Motion Control Design and application experience and profound knowledge of constructing standard and special solutions, Kollmorgen supplies solutions time and again that stand out in terms of performance, quality, reliability, and ease of use. As a result customers can achieve a market advantage which is beyond question. For further information please contact [email protected] or visit our website www.kollmorgen.com
© Kollmorgen.
Use for editorial purposes free of charge. Please note / Request copy from: www.gii.de