Back to top
18 Apr 2014

Attend Interpack 2014 and Learn How to Maximize Design Flexibility and Machine Performance with Reduced Costs, with Kollmorgen AKMH Servo Motors and AKD® Decentralized Servo Drives

RADFORD, VA - Kollmorgen will be exhibiting its family of motion control solutions for packaging machine builders at Interpack 2014, located in Dusseldorf, Germany, from May 8-14, 2014 in the Motion Control and Automation Hall 8a, Stand C 08. Kollmorgen will highlight its new IP69-K rated stainless steel AKMH™ Servo Motor, specifically designed to address the Food Safety Modernization Act (FSMA) and provide long-life and trouble-free operation, even with daily exposure to chemicals and high pressure washdown, The company will also highlight its AKD-N distributed servo drive solution that significantly reduces cabinet space and cabling hassle, simplifying machine design, set-up and operation.

AKMH Servo motor - Hygienic Design"The AKD-N and AKMH solutions can be applied together or separately with other Kollmorgen technologies to take any machine to the next level. AKMH servo motors work with the entire AKD drive platform and AKD-N works with the entire Kollmorgen motor platform, so machine builders can benefit from an exact-fit solution for their specific application needs. These two products are particularly beneficial for packaging machines and will make a new class of simpler and more hygienic machinery," says Tom England, Kollmorgen VP Market Development.

Kollmorgen's AKMH servo motors are specifically designed to reduce the risk of food recall, reduce cleaning time and increase reliability in harsh washdown environments. They feature a hygienic housing design that meets EHEDG, NSF, BISSC and 3A guidelines. The smooth surface design, and use of highly corrosion-resistant 316L stainless steel, decreases the risk of product recalls by reducing the possibility of bacteria growth. The AKMH requires no additional protection and can be sanitized without bagging, covering,  or removing it from the machine. Cleaning time is reduced due to single cable technology and no exposed hardware. Kollmorgen is so confident in the quality and performance that the company backs it with a two year warranty against water ingress -the best warranty in the industry. 

AKD-C/N FamilyKollmorgen's AKD-N distributed servo drive solution provides machine builders with the flexibility to utilize any Kollmorgen motor technology, while still implementing a system that decentralizes the drives into the machine chassis. Because the AKD-N is able to connect to all types of Kollmorgen motor technologies, the solution enables machine designer's to select motors that are perfectly optimized for environment and load requirements. This modular approach also optimizes the thermal properties of the drives and the cabinet, and by being mounted directly on the machine, distributed AKD-N servo drives significantly reduce cabinet volumes and cabling effort - in fact in certain applications, savings of over 80% can be achieved.

Because AKD-N distributed servo technology can be used alongside any servo drive in the AKD platform, AKD-N creates a new high water mark for ease of use in the building process for OEM's and maintainability in the field for end-users. Drives are quickly and easily installed by making three screw lock connections. Traditional panel mount systems involve cable chasing, panel wiring, tagging, and crimping - AKD-N eliminates these requirements.

 

ABOUT KOLLMORGEN

Kollmorgen is a leading provider of motion systems and components for machine builders around the globe, with over 70 years of motion control design and application expertise. Through world-class knowledge in motion, industry-leading quality and deep expertise in linking and integrating standard and custom products, Kollmorgen delivers breakthrough solutions unmatched in performance, reliability and ease-of-use, giving machine builders an irrefutable marketplace advantage.

For more information visit www.kollmorgen.com, email support@kollmorgen.com or call 1-540-633-3545.