Back to top
25 Jun 2007

New SynqNet® Interest Group Established to Promote and Advance Global Adoption in Performance Motion Applications

WOOD DALE, IL – Kollmorgen has established the SynqNet® Interest Group at SynqNet.org as an educational resource for design engineers to maximize the capabilities of the SynqNet technology in their performance motion applications. Members benefit from full access to online and downloadable SynqNet articles, case studies, and flash animations, quarterly e-newsletters on the latest SynqNet news and developments, invitations to annual SynqNet meetings, and direct email access to SynqNet experts. Membership is free and is open to anyone interested in learning more about SynqNet.

“With more than 270,000 axes running worldwide, SynqNet is the most widely utilized motion network in operation today and growing rapidly. As a result, the SynqNet Interest Group was established as an avenue of communication and education to help system and design engineers better understand the advantages of SynqNet system architecture and technology, and how it can help them build a better machine, faster, in performance motion control applications,” says Dean Onishi, SynqNet Communications Manager. Onishi says the group also aims to ensure ease-of-use and interoperability across SynqNet products for OEM’s and end-users.

For more information or to become a member of the SynqNet Interest Group visit www.SynqNet.org.

About SynqNet
The SynqNet motion network was designed to meet demanding motion applications and industry trends toward interoperable, digital machinery. SynqNet uses the standard Ethernet IEE802.3 physical layer for robust isolation and 100m cable lengths with a deterministic protocol engineered by Kollmorgen. SynqNet creates system modularity, HotReplace™ service without downtime, remote diagnostics, software field upgrade, multi-vendor support and fault-tolerant safety. Since 2003, over 300,000 SynqNet axes have been installed. To stay informed with all the latest SynqNet related news, join the SynqNet Interest Group at www.SynqNet.org, where you’ll find technical white papers, case studies, and overviews of all SynqNet products.

About Kollmorgen
Kollmorgen is a leading provider of motion systems and components for original equipment manufacturers (OEMs) around the globe. With over sixty years of motion control design and development expertise, Kollmorgen delivers breakthrough solutions unmatched in performance, reliability and ease-of-use. Through world-class knowledge in motion, industry-leading quality, and deep expertise in linking and integrating standard and custom products, Kollmorgen provides OEMs with the competitive advantage they need to succeed.

For more information visit www.kollmorgen.com, or call 1-540-633-3545.