Back to top
 
 
 

 
 
  Europe | May 2019       
 
 
  Bricks that can put in an appearance  
 
     
 
 
 

Motion Control makes fast and precise cuts from the column of clay

 
 
 

Neat as a pin, each brick on the pallet is identical to the next. Deviations at the building site are accepted only within tight tolerances. Standardized measurements are already in demand simply because bricklayers these days rarely lay the vertically perforated bricks with mortar but glue them together with thin-bed mortar as piece work. Balancing gaps – error reports. And then every deviation from the norm also costs time – which is why manufacturers such as the Swiss brick manufacturer Landquart AG is continuously improving its established production process.

 
 
  Read More  
 
 
  Blog in Motion  
 
     
 
 
 

Is Robotization Destroying or Creating Jobs?

 
 
 

The human vs. robot topic in workplaces has been in the spotlight for quite a while. Look at the comments under the YouTube video where Google introduced its AI (Artificial Intelligence) assistant that could call restaurants and salons to make appointments - there is widespread concern from the audience over the risk of human workers being replaced by AI-equipped machines.

 
 
  Read More  
 
 
  Learn More With Kollmorgen  
 
 
 
 

 

 

 

Success Stories Product Overview Video Gallery Motioneering Online Kollmorgen Developer Network
 
 
 
 
 
  KOLLMORGEN Europe GmbH | Pempelfurtstraße 1 | DE-40880 Ratingen
 Local court Düsseldorf, HRB 35844 | Managing Directors: Jan Treede, Glenn Edward Deegan, Todd Patriacca
Data Processing Information | [email protected] | Unsubscribe