Back to top
 
 
 

 
 
  Europe | March 2019       
 
 
  Frameless direct drive linear motors for metal cutting  
 
     
 
 
 

3D Cutting for large formats

 
 
 

There are few companies around the world capable of building machines that can cut large formats and a variety of materials, including metal, wood, plastic, ceramic, glass, methacrylate, and composite materials. Laser cutting is used successfully where advanced technology, accuracy, and speed are necessary.
KOLLMORGEN direct drive linear and frameless motors, IC and KBM series,enabled to improve performance in terms of thrust and the performance/size ratio compared to the competition to build an extraordinary machine…

 
 
  Read More  
 
 
  Blog in Motion  
 
     
 
 
 

Evolution of the Robot - Hollywood vs Reality

 
 
 

A few years ago Emily Blanchard watched the DARPA challenge. If you’re not familiar with the challenge, the idea was to build a robot that could drive a car, climb a ladder, turn a handle, use a drill and various other activities. In the challenge each robot was given an hour to complete the tasks. 

 
 
  Read More  
 
 
  Precise Motion Control in Meat Processing Applications  
 
     
 
 
 

IFFA - Hall 9.1, booth D74

 
 
 

KOLLMORGEN shows decentralized servo solutions during the international meat processing fair IFFA between May 4 and 9, 2019, in Frankfurt.

 

We are looking forward seeing you!

 
 
  Read More  
 
 
  Learn More With Kollmorgen  
 
 
 
   
 
 
 
  KOLLMORGEN Europe GmbH | Pempelfurtstraße 1 | DE-40880 Ratingen
Local court Düsseldorf, HRB 35844 | Managing Directors: Jan Treede, Guido Markus Reinke
Data Processing Information | datenschutz@kollmorgen.com | Unsubscribe