Back to top
 
 
 

 
 
  Europe | Oct '17  
 
 
  The risk with vertical axes  
 
     
 
 
 

Monitoring and controlling brakes are part of functional safety technology at KOLLMORGEN

 
 
 

Safety of people and machinery is a constant challenge, particularly with applications that involve loads transported and positioned vertically. There are challenging issues that arise from the design to the construction stages especially when the goal involves ensuring the safety of vertical axes with high loads using just the holding brake installed in the drive motor.

 
 
  Read More  
 
 
  Comau’s first AGV:  
 
     
 
 
 

A flexible Solution for the SMART factory

 
 
 

The result of this collaboration is “AGILE 1500” Comau’s first ever AGV: scalable, fully on-line and customizable, able to adapt to multiple navigation systems. A solution in keeping with the status of Industry 4.0.

 
 
  Read More  
 
 
 
  Blog in Motion  
 
     
 
 
 

Issues to Consider when Operating a Motor in a Vacuum

 
 
 

Question: I need to operate a servo motor in a vacuum, what are some considerations?


Answer: In a word? You might think that proper motor sizing* is a big issue, it always is, however...

 
 
  Read More  
 
 
  Learn More With Kollmorgen  
 
 
 
   
 
 
 
  KOLLMORGEN Europe GmbH, Pempelfurtstraße 1, 40880 Ratingen
Privacy Statement | Site Disclaimer