Back to top
 
 
 

 
 
  Europe July 2017  
 
 
  A perfect solution in Bakery Automation  
 
     
 
 
 

For the pre-ferment, Bühler has developed a solution

 
 
 
 

No hearty rye bread without sourdough. The stollen becomes deliciously soft when some of the baking ingredients are first mixed together and left to rise (thanks to the properties of yeast) before all the other ingredients are blended into the main dough. The mixture made mainly from cereal flour and bulk liquids such as water and milk is known as pre-ferment among bakers.

 
 
  Read More  
 
 
  Youtube Video  
 
     
 
 
 

AKM DC Servo Motor low voltage for autonomous vehicles

 
 
 
 

With the Packman 200, Opteq Robotics has developed a self-driving solution for material flows which makes its way quickly and directly through the aisles to reach its destination, just like the popular arcade game from the 1980s.

 

 
 
     
 
 
 
  Blog in Motion  
 
     
 
 
 

Food Recall Hits Close to Home

 
 
 
 

On February 21st, a recall for a soft cheese was issued due to high amounts of Listeria monocytogenes. Virginia and Maryland have been investigating the products from the manufacturer.

 
 
  Read More  
 
 
  Learn More With Kollmorgen  
 
 
 
 
  Success Stories Product Overview Video Gallery Motioneering Online Kollmorgen Developer Network
 
 
         Request a Quote
 
 
  KOLLMORGEN Europe GmbH, Pempelfurtstraße 1, 40880 Ratingen
Privacy Statement