Back to top
 
 
 

 

 
 
  Europe 23 Feb '17  
 
 
  Decentralized drives on the rotary table  
 
     
 
 
 

Safety via the slip ring

 
 
 
 

KOLLMORGEN is bringing its AKD-N decentralized servo drives to the rotary table. Less cabling, less mass, less work – these are just three advantages of this solution. Control, performance and safety are incidentally transmitted via the slip ring. The drive in our trade show exhibit: A direct drive from KOLLMORGEN’s KBM Series – the frameless direct drive is controlled by the PCMM Motion Controller.

 

 
 
     
 
 
  Decentralized vs. centralized control technology  
 
     
 
 
 

Specialist lecture by Dr. Arne Linder at all about automation

 
 
 
 

“What is the effect of shifting the drive technology from the control cabinet to the machine?” Dr. Arne Linder will address this question in his technical lecture during the trade show “all about automation” on March 8/9, 2017 in Friedrichshafen. The product manager of Drives at KOLLMORGEN is giving his lecture on both days of the trade show in the Talk Lounge (hall A2, stand 130): Wednesday at 2 PM and Thursday at 10 AM.

 
 
     
 
 
 
  New generation of servo drives by Lake Constance  
 
     
 
 
 

EAT and KOLLMORGEN at ‘All about automation’ in Friedrichshafen

 
 
 
 

It would be great to know about everything the next generation of servo drives can do: this is why EAT and KOLLMORGEN will be exhibiting the new AKD2G servo amplifiers at "All about automation" – a two days‘ event in Friedrichshafen. The automation trade fair for users in the international Lake Constance region is to be held on March 8th and 9th, 2017, at Messe Friedrichshafen. EAT and KOLLMORGEN will be exhibiting at Stand 325 in Hall A2.

 
 
  Read More  
 
 
  Learn More With Kollmorgen  
 
 
 
 
  Success Stories Product Overview Video Gallery Motioneering Online Kollmorgen Developer Network
 
 
         Request a Quote
 
 
  KOLLMORGEN Europe GmbH, Pempelfurtstraße 1, 40880 Ratingen
Privacy Statement