Back to top
 
 
 

 
 
  Europe March '17  
 
 
  Centralized or Decentralized?  
 
     
 
 
 

Which architecture type delivers the best technical and commercial advantages?

 
 
 
 

Decentralizing servo technology can bring machine and plant construction savings during installation. Two additional advantages include reduced cabinet heat loads and more straight forward drive architecture. The question arises however, which technology is better, an integrated motor/drive solution or a detached motor and drive?

 
 
  Read More  
 
 
  Blog in Motion  
 
     
 
 
 

Modbus TCP with AKD Compared to Fieldbuses

 
 
 
 

Unlike fieldbus communications only being supported by particular models of the AKD servo drive, Modbus TCP communication is supported by all of the AKD models. Whether you have a simple "analog" drive, an indexing drive...

 
 
  Read More  
 
 
 
 
  Amper Tradeshow in Brno, Czech Republic  
 
     
 
 
 

21 to 24 March 2017 - Stand: V 6.11

 
 
 
 

During the exhibition Amper in Brno, Czech Republic, Raveo s.r.o. displays advanced motion technologies from KOLLMORGEN on its stand.

 
 
     
 
 
  Learn More With Kollmorgen  
 
 
 
 
  Success Stories Product Overview Video Gallery Motioneering Online Kollmorgen Developer Network
 
 
         Request a Quote
 
 
  KOLLMORGEN Europe GmbH, Pempelfurtstraße 1, 40880 Ratingen, Germany
Privacy Statement