Back to top
 
 
 


 
 
  Europe April '16  
 
 
  Magnetic field instead of feed rollers  
 
     
 
 
 

tecodrive is developing a revolutionary process for material feed applications with the help of servo drives from Kollmorgen.

 
 
 

tecodrive GmbH from Garbsen has named its invention "fleXfeed" – and is breaking revolutionary new ground in material feed applications used for metal processing. Thanks to an ingenious magnetic field, "fleXfeed" works on a completely contact-free basis and is much faster than conventional feed rollers.

 
 
  Read More  
 
 
  Safe encoder  
 
     
 
 
 

KOLLMORGEN combines AKM motors with safe feedback

 
 
 

There are now two new certified safety feedback systems for AKM servo motors in the form of sine/cosine encoders (Hiperface) for single-turn and multi-turn applications.

 
 
  Read More  
 
 
 
  Precise Motion Control in Meat Processing Applications  
 
     
 
 
 

IFFA - Hall 11, booth D21

 
 
 

KOLLMORGEN shows decentralized servo solutions during the international meat processing fair IFFA between May 7 and 12, 2016, in Frankfurt.

 
 
  Read More
 
 
 
  ICH Direct Drive Linear Motor Selection Guide Update  
 
     
 
 
 

The ICH series of maintenance-free iron-core linear motors offer high power density and transmit it without any mechanical components. The units are designed so as to deliver feed forces between 175 and 5341 N in continuous operation (maximum force more than 12,000 N).

 
 
  Download
 
 
  Learn More With Kollmorgen  
 
 
 
   
 
 
 
  KOLLMORGEN Europe GmbH Pempelfurtstraße 1 DE-40880 Ratingen
Privacy Statement | Unsubscribe
 
{{^Account.ADDRESS(KOLLMORGEN Europe GmbH)}}