Back to top
 
 
 

 
 
  Europe 28 Jan '16  
 
 
  Free choice: AKM Servo Motor now with DRIVE-CLiQ  
 
     
 
 
 

KOLLMORGEN combines its servo motors with SiemensWorld

 
 
 

KOLLMORGEN AKM servo motors are now available as DRIVE-CLiQ versions. The price and performance advantages of AKM synchronous servo motors can be harnessed directly for CNC applications with Sinumerik control in metal processing – without having to compromise in terms of the connection technology

 
 
  Read more  
 
     
  Max Speed and Energy Efficiency with Hybrid Design  
 
     
 
 
 

First in Turkey in the field of Plastic Injections,

 
 
 

Tisse and Kollmorgen have together developed an electric-hydraulic Hybrid Machine. The Hybrid Machine can manufacture difficult and sensitive products at high speeds;....

 
 
  Read more  
 
     
  Partner of the Year 2015  
 
     
 

 

 
 

IBD GmbH from Munich/Germany and Delta Elektronik from Taastrup/Denmark,

 
 
 

the two European partner prizes awarded by KOLLMORGEN form a North-South axis in 2015.
At sps ipc drives 2015 Managing Director Franz Hangl accepted the "Partner of the Year 2015" award on behalf of ibd GmbH from CEO Dan St. Martin and Managing Director for Germany, Jan Treede.

 
 
  Read more  
 
     
  Blog in Motion  
 
     
 
 
 

Ethernet Networks Simplified

 
 
 

Setting up an Ethernet network can be frustrating if you don't understand the basics. A network is just the communication connection between two or more devices. These devices can be computers, PLC's, servo drives,...

 
 
  Read more  
 
     
  Sign up now: FREE Webinar  
 
     
 
 
 

Food Safety Update: Using the Joint Collaboration Process to Implement New Criteria for Hygienic Equipment Design for Low-Moisture Foods

 
 
 

This Free PMMI’s OpX Leadership Network webinar is sponsored by KOLLMORGEN and includes a Live Q&A
25th of Feb 2016 – 12:00 PM (US Eastern Time)*

 


*If you are not able to attend live, you can view the webinar after registration on demand 

 
 

 
  Learn More With Kollmorgen  
 
 
 
 

 

 

 

Success Stories Product Overview Video Gallery Motioneering Online Kollmorgen Developer Network
 
 
 
 
 
  KOLLMORGEN Europe GmbH Pempelfurtstraße 1 DE-40880 Ratingen
Privacy Statement | Unsubscribe