Back to top

360 degree labeling with direct drive

Joint development: Motion control solution with integrated labeling controller

Ever more mobile electronic devices are firing up the consumption of batteries and rechargeable batteries - according to GfK from 116 million in 2008 to 300 million in 2012 in Germany alone. In light of these figures from the German consumer research association, productivity is crucial for cost-efficient production. During a redesign of the system, Schleuter mechanical engineers managed to increase the output of an existing battery labeling machine in China from 600 to 1000 units per minute. This increase was possible thanks to an automation including Motion Control that was integrated into the Kollmorgen drive control system.

 

Kollmorgen Schleuter AKD PDMM Servo Drive
 

 

Also interesting for a colleague? Simply forward this email...            

KOLLMORGEN Europe GmbH | Pempelfurtstr. 1 | D-40880 Ratingen | www.kollmorgen.com | 
+49.(0)2102.9394.0  | [email protected]

eNews subscribe | eNews unsubscribe | eNews - Archive | Privacy Statement

©2014 Kollmorgen. All rights reserved.