Back to top

Kollmorgen eNews

 

Kollmorgen Automation Suite version 2.8 delivers new functions

Kollmorgen AKD PDMM Servo Drive

With an embedded EtherCAT configuration tool, version 2.8 of the Kollmorgen Automation Suite (KAS) software accelerates the development of modular machine architectures. The new release of the integrated development environment enables users to build complete EtherCAT systems and configure all peripheral components, including HMI, I/O, controllers and motors, with a single tool. The resulting simplification along with ergonomic improvements, makes life easier for system developers and increases engineering efficiency.
One of the key innovations in Kollmorgen Automation Suite 2.8 is the embedded EtherCAT configuration tool, which makes it easy to integrate EtherCAT components (including those from other manufacturers) into the application. With this open architecture, Kollmorgen reduces development time for modular, multi-purpose machine architectures. Another clear advantage of this approach is that direct communication with Kollmorgen AKD PDMM servo controllers from PC-based applications is now possible using UDP and HTTP protocols.

Sindex, Bern: KOLLMORGEN shows off future machine design

Visit Kollmorgen at the Sindex

Solutions with the essentials in mind – that is what’s behind KOLLMORGEN’s approach to Simple Machine Design. At the Sindex trade fair in Bern, the experts in servo drive technology and motion control will be demonstrating why simplicity is new spirit in machine and plant construction. From September 2 – 4, 2014, KOLLMORGEN will be showcasing its latest innovation at the leading Swiss automation trade fair.

 

Also interesting for a colleague? Simply forward this email...

 

 

 

KOLLMORGEN Europe GmbH | Pempelfurtstr. 1 | D-40880 Ratingen | www.kollmorgen.com | 
+49.(0)2102.9394.0 | think@kollmorgen.com

eNews subscribe | eNews unsubscribe | eNews - Archive | Privacy Statement

©2013 Kollmorgen. All rights reserved.