Back to top

Kollmorgen eNews

 

 

Gallagher takes over from Panenka

Dennis Gallagher Kollmorgen Europe GmbH

Change of leadership: After six successfull years with Kollmorgen, most recently as the Vice President and General Manger for Europe and India, Udo Panenka is moving to ESKO (a Danaher Company) as the Senior Vice President, Global Sales.
Dennis Gallagher is taking over as the Vice President of KOLLMORGEN Europe from Udo Panenka. Dennis comes to KOLLMORGEN Europe with 25 years of motion control and automation experience, he will be at the helm in Ratingen from September 2014.
Dennis Gallagher joined Danaher in 1989 with the acquisition of Pacific Scientific. Most recently, Dennis held a dual role as Vice President and General Manager for both Kollmorgen Medical / Lab Automation and the Dover business.

SPS IPC Drives: “Intelligent Motion” – a key aspect for KOLLMORGEN

Kollmorgen @ sps ipc drives 2014

In the end everything is simple: If primary requirements such as “simple", “efficient” or “connected” are mentioned when equipping a plant, we lose focus on technology in favor of a broader view of things. What can drive and control technology provide here? This is the question that KOLLMORGEN will consider during the SPS IPC Drives Exhibition from 25 to 27 November 2014 in Nuremberg (Hall 3a, Stand 230).

Also interesting for a colleague? Simply forward this email...

 

 

 

KOLLMORGEN Europe GmbH | Pempelfurtstr. 1 | D-40880 Ratingen | www.kollmorgen.com |
+49.(0)2102.9394.0 | [email protected]

eNews subscribe | eNews unsubscribe | eNews - Archive | Privacy Statement

©2013 Kollmorgen. All rights reserved.